FPGA 

Industrial Communication: Industrial Ethernet, TSN, OCP/UA

Critical advantage in industrial communications
Even better than ASSPs, FPGAs hold a critical advantage in industrial communications as all protocols in this field can be implemented in an FPGA with a high degree of flexibility. Industrial Ethernet is a prime example of this. EBV Elektronik has been active in this field for many years for example with its Mercury or new SoCrates platform, with different development platforms, customers can easily evaluate and test different protocols such as EtherCAT, Ethernet/IP, Powerlink, ProfiBus, ProfiNet, Sercos III for their applications. With Industry 4.0, deterministic Ethernet (TSN) will first be used on PLC to PLC communication using OPC/UA, but has a good chance to be used in devices as well. EBV provides with its suppliers solutions for today’s requirements which are ready for tomorrow’s needs.

Learn More

PLC - Programmable Logic Controller

A factory control network is based on PLCs which require support for multiple specialised peripherals using an FPGA

They are configured around an application processor that runs the factory control software along any master communication protocol stack.

Learn More

Video Compression

Broadcast, machine vision, surveillance cameras

Also in some consumer display screens, ASSPs, microprocessors, FPGAs and DSPs are used for additional features. Other standards like JPEG, JPEG2000, MPEG can also be implemented in those devices, esp. perfectly suited, when special features like low latency or non-mainstream resolutions are required.

Learn More

Electrical Drives and Motor Control

EBV Elektronik has already developed several reference designs in the field of drive controls

EBV Elektronik has already developed several reference designs in the field of drive controls. One of the best-known reference designs is FalconEye, in which highly effective and dynamic drive controls algorithms are mapped to the hardware and software of an FPGA. Not only does the FPGA manage the drive control itself, it also performs the industrial communication, for example via a fieldbus including all necessary protocols, and additionally handles the encoder feedback. The wide portfolio of DSPs and microcontrollers complements this offering to find the best solution for a specific requirement.

Learn More

Development Tools

Development tools for several applications are available from EBV, based on Intel FPGA technology

With the appropriate reference boards, customers can easily test different solutions and start implementing their design without the need to build a complete testhardware. This usually saves a lot of time.

Learn More

Technologies around FPGA

FPGAs provide the ideal platform to solve a lot of applications. However to extend the functions and get a complete system solution, there are more technologies required for a complete heterogeneous processing platform

EBV Elektronik offers a wide portfolio of devices from Clock Distribution & PLL, Interfaces, Memory, Power Management, ADC/DAC, Signal Chain and Optical Isolation devices.

Learn More

System Solutions

With the appropriate reference boards, customers can easily test different solutions and start implementing their design without the need to build a complete test hardware

This usually saves a lot of time. After registering,developers will be able to communicate with our design experts by sharing block diagrams within our ‘Build Your Block Design’ tool.

Learn More