HEALTHCARE

Insulin Pump

Insulin pumps deliver rapid- or short-acting insulin 24 hours a day through a catheter placed under the skin

An insulin pump is attached to the skin of the patient. The pump delivers insulin into the body via a cannula. Control of the micro-motor is provided by a microcontroller, which also contains the required programming interfaces. The battery management system ensures the longest possible run time for a single charge.

Blood Glucose Meter

Blood glucose meter is recommended for all people with diabetes as it is a valuable diabetes management tool which can help to give you a sense of control and freedom

In addition to a special integrated front-end IC, blood glucose measurement devices also need a low-to-medium performance microcontroller, a small display and a circuit for battery management. Some devices also contain various wireless interfaces for transferring values to a computer or a Telehealth Hub.